This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1312R1: TI-15.4 Collector Stack getting ApiMac_status_badState from the Coprocessor

Part Number: LAUNCHXL-CC1312R1

Tool/software:

Hi,

We have a Linux Collector Host Application talking to a MAC Coprocessor running on a LAUNCHXL-CC1312R1 device.

The Linux Collector Stack version we are using is: [4.10.00.06].

We sometimes come across an indication of BAD STATE when communicating between the Linux Collector and the Coprocessor.
The return status from the Collector API_MAC_TxRx_Status() function is using the MT based interface function MT_MSG_txrx ().
The comment in the code only says: /* Something is wrong... */. I understand that the transmission to and from the Coprocessor was not fully successful but is there a way to get the exact reason for such failure?
Thanks for the help.
Siham.