This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200: CC1200

Part Number: CC1200

Tool/software:

Hi,

We encountered an issue while debugging CC1200. There are three types of data transmission communication modules, one of which is a chip from another manufacturer with an unknown model and the datarate is 9600, FDEV=4KHz, The frequency is 460MHz, numbered as 1; One is a data transmission communication module based on CC1200 developed by other companies, with the datarate 9600, FDEV=2.4KHz, The frequency is 460MHz, numbered 2; The last one was made by ourselves based on CC1200, with datarate 9600, FDEV=2.4KHz, The frequency is 460MHz, and numbered as 3. Number 2 can communicate with Number 1, while Number 3 cannot communicate with Number 1. We need technical support. Is there any parameter that hasn't been set correctly?

thanks!