Other Parts Discussed in Thread: UNIFLASH, BLE-STACK
Tool/software:
Hello,
I am trying to store some data in the NVS memory area.
To get the code running I used the code from the nvsinternal_CC1352R1_LAUNCHXL_tirtos_ccs example project.
This project uses the NVS.h driver functions.
Writing and reading works fine, but the memory area is altered after a power reset.
I am not using the debug mode since I read that it kills the nvs area as a default but connect to the already running target to watch my arrays and varialb

}
bool nvs(void)
{
uint16_t offset = 0x50; //how do I know this does not clash with the bonding table?
uint8_t readnvsData[8];
static const uint8_t data[8] =
{0x0F, 0x42, 0x3F, 0x5A, 0x5A, 0x5A, 0x5A, 0x5A};
bool res = true;
NVS_Handle nvsHandle;
NVS_Attrs regionAttrs;
NVS_Params nvsParams;
NVS_init();
NVS_Params_init(&nvsParams);
nvsParams2 = nvsParams;
nvsHandle = NVS_open(CONFIG_NVSINTERNAL, &nvsParams);
if (nvsHandle == NULL) {
res = false;
}
NVS_getAttrs(nvsHandle, ®ionAttrs);
int_fast16_t resRead = NVS_read(nvsHandle, offset, (void *) readnvsData, sizeof(readnvsData)); // on first boot the bytes read here are all 0xFF, after power reset they should match the ones written below
resRead = NVS_write(nvsHandle, offset, (void *) arrayToWrite, 8, NVS_WRITE_ERASE | NVS_WRITE_POST_VERIFY);
resRead = NVS_read(nvsHandle, offset, (void *) readnvsData, sizeof(readnvsData)); // matches the written data from a column above
NVS_close(nvsHandle);
return res;
}
The content of the read array after the power reset:

I am calling this function right after the startup before BIOS_start();
I am not sure if the usage of the NVS driver is correct here since I saw that most people in the forum seem to use the oasl function which didn't work for me.
I read somewhere that some devices only allow multiples or 4 bytes for the write operation.
Is this true for the CC1352R?
So far I see that no other module is using the NVS driver, can there be some settings somewhere though that could mess up my memory? The bondmanager perhaps?
I also played with the offset value, setting it to 0x2000 or 0x50 but the result stays the same.
Is there something I need to do before the power reset to lock the memory permanently?
We use SimpleLink CC13x2 26x2 SDK v5.20.0.52 and cannot update to a newer one.
Thanks for the support
Miriam