Part Number: CC1352R
Hi,
we are working on a design with the CC1352R and we are using the internal DCDC Converter.
Between DCDC_SW and VDDR_RF an inductor is required. What are the electrical requirements of the inductance?
I know that the technical documentation referes to the reference design with the MLZ2012N6R8LT000, but due to space limitation we can only use smaller ones. Also in case of second source issues, there is a need for gerneral requirements to the Inductance.
In the technical reference manual there are information that allows conclusions to be drawn about certain parameters.
in Table 11-4:
- inductor current: 46mA to 87mA?
- "Assuming 10µH external inductor!" --> 6,8µH or 10µH?
or in Table 7-10
- DCDC clock source 48MHz --> On which switching Frequency is the DCDC running?
best regards
Fabian