This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101 FIFO TX

Other Parts Discussed in Thread: CC1101, TEST2

I am using two cc1101 for Tx and Rx in 410 Mhz. I set Rx in asynchronous mode and Tx in FIFO mode. When I send data in 100 Kbit/s by FIFO I can receive data on GDO0 pin in receiver but when I send data in 500 Kbit/s by FIFO I can't receive data.
I check by spectrum analyzer and see signal spectrum. In 100Kbit/s I can see FSK signal  but in 500kbit/s I see carrier with lines similar pulse signal spectrum.

100 kBits/s



500 kBit/s


This is my code (SPI CLK is 8 Mhz):


#define FSCTRL1_val 0x06                // Frequency synthesizer control.
#define FSCTRL0_val 0x00                // Frequency synthesizer control.
#define FREQ2_val 0x0F                  // Frequency control word, high #define.  Fc=410 mhz
#define FREQ1_val 0xC4                  // Frequency control word, middle #define.
#define FREQ0_val 0xEC                  // Frequency control word, low #define.
#define MDMCFG4_val 0x0E               // Modem configuration.
#define MDMCFG3_val 0x3B               // Modem configuration.
#define MDMCFG2_val 0x10                // Modem configuration.
#define MDMCFG1_val 0x01                // Modem configuration.
#define MDMCFG0_val 0xF8                // Modem configuration.
#define DEVIATN_val 0x75                // Modem deviation setting (when FSK modulation is enabled).  Deviation=50 khz
#define FREND1_val 0x56                 // Front end RX configuration.
#define FREND0_val 0x10                 // Front end RX configuration.
#define MCSM2_val 0x0A                  // Main Radio Control State Machine configuration
#define MCSM1_val 0x3C                  // Main Radio Control State Machine configuration
#define MCSM0_val 0x08                  // Main Radio Control State Machine configuration
#define FOCCFG_val 0x16                 // Frequency Offset Compensation Configuration.
#define BSCFG_val 0x6C                  // Bit synchronization Configuration.
#define AGCCTRL2_val 0x03               // AGC control.
#define AGCCTRL1_val 0x40               // AGC control.
#define AGCCTRL0_val 0x91               // AGC control.
#define FSCAL3_val 0xE9                 // Frequency synthesizer calibration.
#define FSCAL2_val 0x2A                 // Frequency synthesizer calibration.
#define FSCAL1_val 0x00                 // Frequency synthesizer calibration.
#define FSCAL0_val 0x1F                 // Frequency synthesizer calibration.
#define PKTCTRL1_val 0x88               // Packet automation control.
#define PKTCTRL0_val 0x00              // Packet automation control.
#define PKTLEN_val 0x3C                 // Packet length.
#define IOCFG2_val 0x0D                 // GDO2 output pin configuration
#define IOCFG1_val 0x2E                 // GDO1 output pin configuration
#define IOCFG0_val 0x06                // GDO0 output pin configuration

#define FSTEST_val 0x59                 // Frequency synthesizer calibration control
#define CHANNR_val 0x00                 // Channel number.
#define TEST2_val 0x88                  // Various test settings.
#define TEST1_val 0x31                  // Various test settings.
#define TEST0_val 0x0B                  // Various test settings.
#define ADDR_val 0x00                   // Device address.
#define FIFOTHR_val 07                  // RX FIFO and TX FIFO thresholds
#define SYNC1_val 0xD3                  // Sync word, high byte
#define SYNC0_val 0x91                  // Sync word, low byte                
#define WOREVT1_val 0x87                // High #define Event 0 timeout
#define WOREVT0_val 0x6B                // Low #define Event 0 timeout
#define WORCTRL_val 0xFB                // Wake On Radio control
#define RCCTRL1_val 0x41                // RC oscillator configuration
#define RCCTRL0_val 0x00                // RC oscillator configuration
#define PTEST_val 0x7F                  // Production test
#define AGCTEST_val 0x3F                 // AGC test


void send_packet (unsigned char length,unsigned char send_data[]){
write_burst_reg(FIFO,length,send_data);
write_strobe(STX);                 // send data into the transmit mode
while (!VPORT3_IN.0)            // Wait for GDO0 to be set -> sync transmitted
write_strobe(SNOP);
while (VPORT3_IN.0);
write_strobe(SIDLE);
write_strobe(SFTX);
}

for(q=0;q<62;q++)
pulse[q]=0x55;
delay_us(100);
SET_SPIC_SS_LOW;
while(VPORT2_IN.6);
write_strobe(SRES);
while(VPORT2_IN.6);
RF_setting();
delay_us(100);
write_strobe(SCAL);
delay_us(900);    
while (1)
      {     
      send_packet (60,pulse);

      }

}

What is the problem in 500Kbit/s ?

Thanks for helps

Best Regards