Hi all,
I am attempting to interface an MSP430F1611 to a 950/960 MHz CC1100E, but I cannot get the pair to transmit properly.
On the transmitting side, I have a CC1100E evaluation module plugged into a SmartRF04 evaluation board, which is then connected to an MSP430F1611 breakout board. The relevant resistors on the evaluation board have been removed, and the connections I've made are as follows (evaluation board -> MSP430):
G0 -> P2.4
G2 -> P5.6 (connected but not used)
CSn -> P5.4
SCLK -> P3.3
SI -> P3.1
SO -> P3.2
GND -> GND
I've double checked these connections but I put them here in case there's something obvious I've missed. On the receiving side, I have an unmodified SmartRF04 evaluation board plugged into a PC and connected to SmartRF Studio 7.
To set the CC1100 registers on the transmitting board, I went to the SmartRF Studio Easy Mode, selected the 955 MHz low data rate packet tx configuration, and exported the register settings to my code. The receiving registers are the defaults set by SmartRF Studio. My process is to start packet RX on the receiving module, and then run the tx code on the microcontroller. However, the receiving module never receives any packets.
Debugging further, I found that the microcontroller hangs on this line in the code from the library:
while (!(TI_CC_GDO0_PxIN&TI_CC_GDO0_PIN));
... showing that GDO0 doesn't go high when transmitting. I am somewhat of a beginner at this I have no idea what the problem could be, can someone please point me in the right direction? Unfortunately, I do not have a logic analyzer available to double check the SPI communication, but I do have an oscilloscope. I have included my main.c code below, but I can post other files or register settings if requested.
Thanks in advance for any help!
// CC1100 Test
#include "include.h"
extern char paTable[]; // Defined in CC1100-CC2500.c
extern char paTableLen;
char txBuffer[4]; // Send buffer
char rxBuffer[4]; // Receive buffer
void main(void){
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog
// Initialize LED
P6DIR |= BIT0;
P6OUT |= BIT0;
__delay_cycles(5000); // 5ms delay to compensate for different startup times
// Setup SPI & CC1100
TI_CC_SPISetup(); // Initialize SPI port
TI_CC_PowerupResetCCxxxx(); // Reset CC1100
writeRFSettings(); // Write RF settings to CC1100. RF settings can be gathered from SmartRF Studio 7 & entered into CC1100-CC2500.c
// Write power amplifier table. Value taken from SmartRF Studio
TI_CC_SPIWriteBurstReg(TI_CCxxx0_PATABLE, paTable, paTableLen);
// Build packet
txBuffer[0] = 2; // Packet length
txBuffer[1] = 0x01; // Packet address
txBuffer[2] = 0x2A; // Packet content
unsigned int i;
for(i=0;i<10;i++){
RFSendPacket(txBuffer, 3); // Repeatedly send packet
P6OUT ^= BIT0; // Turn on LED
}
// Wait
P6OUT ^= BIT0; // Turn on LED
while(1){}
}