Hi,
Is it possible with CC2530 to bypass Tx/Rx calibration steps and associated 192usec delay and go directly to "Tx" (34-38) or "SFD wait" (3-6) states, according to radio state machine? I assume there should be some "undocumented" command strobes to do this. This should give ~4% RF power saving - for example for bursts over same channel when calibration is needed only for the first packet (and/or VCO_CAPARR/etc. values are calibrated/preloaded manually).
Thanks,
Igor