Is there a balun that can be used with the CC1310 at 868MHz?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We have had this discussion with both Johanson and Murata for a CC1310 IPC at 433 MHz. Previously, 433 MHz IPCs have not been too popular so this is more business based decision from Johanson or Murata if the IPC will be developed.
Regards,
Richard
I am curious why there is an extra capacitor (C15 or C16) in swra524a compared to the CC112x IPC reference design. Was this added because the IPC did not perform as expected? Is this capacitor needed for both Murata and Johanson parts?
EDIT: this is explained on page 4, there is no built-in DC blocking in the IPC. Can you confirm that the CC112x IPC does have DC blocking, and no extra capacitor is needed in that case?
Also, there is a typo in swra524a on page 5. It says "overall footprint area for all the required components is less than 0.94 mm2", which should be cm2.
Hi Andrew,
For the CC13xx IPC, the DC block capacitors could not fit into the ceramic package. If the DC block would of been included, then we would be forced to use a larger ceramic package size for the design. A larger ceramic size would of increased the cost so the DC blocking capacitor was chosen to be external.
The CC112x discrete ref design inherently contains the DC blocking caps and the IPC is the equivalent circuit. In the CC112x IPC ref design a 100 pF capacitor is used as a switch in the position of C202. I'm double checking that there is no need for a DC blocking cap and will reply with confirmation very soon.
0.94 mm2 is a typo.
//Richard