Hello,
I would like to verify that I understand the CC115L datasheet correct.
On page 38 under "Table 5-12. GDOx Signal Selection (x = 0, 1, or 2)" in last row:
"(0x2F) HW to 0 (HW1 achieved by setting GDOx_INV=1). Can be used to control an external PA."
HW means hardwired right?
so if set 0x2F to the IOCFG2 register (GDOx_INV=0) than GDO2 should be hardwired to zero.
Is this correct?