Hi,
How to flash both BLE stack + TI15.4 stack so the smartphone can communicate with CC1350 and CC1350 be part of a 802.15.4 network?
Cheers,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
How to flash both BLE stack + TI15.4 stack so the smartphone can communicate with CC1350 and CC1350 be part of a 802.15.4 network?
Cheers,
Hi,
we just released CC1350 to the market, which is a great dual-band device and the first to come with an integrated system offering solutions and arbitration between different bands and modulation is done through a dual-band RF driver.
While as of today the dual band functionality is supported through the RF driver and demonstrated via RF EasyLink examples, we obviously expand to add support for more things in the future. I can't disclose much more roadmap information on the public forum (please contact a TI representative for more information) however we see that both standard stacks networking solutions like 15.4 Stack and proprietary RF are both Sub-1 GHz technologies where the integration with BLE makes lot of sense for several use cases (like beaconing or commissioning).
Please stay tuned! More is to come.
Thanks,
TheDarkSide
Hi, is it possible to replace the Esaylink with Prop RF APIs such as RF_runCmd in the rfWsnDmNode demo project?