This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding LAUNCHXL-CC1350 - Antenna and Simultaneous use of Sub-1 and 2.4 GHz radio

Other Parts Discussed in Thread: LAUNCHXL-CC1350, CC1310, CC1350

I have just ordered Launchxl-cc1350 and started playing with it. I had a couple of questions which may be quite naive.

1. The range for line of sight communication is mentioned to be around 20km on a coin cell. Is there some external antenna that is suggested to be used to get such long range communication? Link to tutorial or discussion anywhere would be really helpful to get started.

2. It is said to support both Sub-1 and 2.4GHz communication. Does it mean that it has 2 dedicated radios? If not, can the application change in real time to make use of either of the frequencies depending on need?

Thanking you all in advance :)

Best regards,

Mobashir