Other Parts Discussed in Thread: MSP430F1611,
Hello to everyone!
We have a system based on the MSP430F1611 and the CC1101-CC1190 and we want to receive radio frames from some sensors that are based on the radio chip AX5043 of AXSEM.
Physically, they have the same configuration, and aparently the framing header (preamble + syncword+length+address, NO CRC on both) are the same, but we don't receive anything from the sensors. We have changed on the CC1101 the header configuration (non preamble, 16 bits of preamble, 32 bits, etc) , the addressing matching, etc; well, we are in the fase of try and error. On the sensors side, I am afraid that we can't change their configuration.
With the Spectrum Analyzer we compare the sensors and our system signals and they are tuned on the same base frequency (869.4MHz) so we think that the problem is on the framing identification. Anyone knows if the CC1101 and AX5043 are compatible?
Thanks in advance!!
PD: In the image, the green signal is emitted by the sensors (AX5043) and the yellow one is our signal.
Best regards,