This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: How to send data in long range mode

Part Number: CC1310

Hi all,

I want to send data minimum range of 1km (line of sight). My data rate is up to 10kbps. I used 2-GFSK, 30kbps stmbol rate, 15kHz deviation, 59kHz RX BW and i reach to 300m.

There are few typical settings in SmartRF Studio 7, Version 2.6.0 such as :

Q1: In here, i know there are so much differences between long range mode and 50kbps mode. I observe differences using code export. But what are the differences between 50kbps and 10kbps mode except deviation, symbol rate and rx BW filter?

Q2: Which rf settings can you suggest to me to provide these specs(1 km range and 10kbps max data rate)?

Q3: Using SmartRF Studio 7, i exported code of 10 kbps typical setting and loaded these code settings to my CC1310. But with these settings CC1310 cannot send any data. But when i loaded the codes of 50kbps typical setting CC1310 can send data. What can be reason of this problem? Is 10kbps mode incompatible with my CC1310 chip?

Q4: When i connect to CC1310 Launchpad using SmartRF Studio 7 these settings are observed in SmartRF studio.

When i connect to my custom CC1310 board using SmartRF Studio there settings are observed.

So Does it mean my board cannot support other typical settings such as 10kbps and 5kbps Long range modes ?

Best Regards.

Thank you.