Other Parts Discussed in Thread: CC1310
Greetings
I have troubles with making a project based on cc1350 chip. I cannot even upload an example using XDS110 (part of cc1350 LP). At the end of uploading i get this error:
Status: Cortex_M3_0: Can't Run Target CPU: (Error -2134 @ 0x0) Unable to control device execution state. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.576.0)
What exactly is ment by "lower TCLK"? Or how do i fix this error?
And the other question was regarding capacitors used in electrical circuit of cc1350LP. (shown in a picture C6, C8)
Are they really suppose to be 22uF? I cant really find any 22uF SMD capacitors. Is it a correct value?