Other Parts Discussed in Thread: CC1350
Hello,
I am trying to create 6lowpan network with 1. CC1350+ENC28J60 as Edge router 2. CC1350 as End node
I refereed
which covers my first requirement of edge router using cc1350+enc28j60 and it is running successfully.
Now for the second part I wanted to know which program will be compatible to run on cc1350 as node and communicate with the router?
If there is no program available then which program do I need to modify and what changes should be done.
Thanks.