Other Parts Discussed in Thread: CC1021, CC1125, CC1120
Hi,
I am looking for a RF transceiver part similar to CC1000. CC1000 is not recommended for new designs according to TI website. The recommended parts are not meeting my requirements.
I am looking for a pue RF transceiver operating within the range of 920MHz-1050MHz wihtout any specific modulation/demodulation protocol.
I need to have the RX analog IF outputs so that i can have an external ADC. Also, I need to be able to bypass any internal AGC and set the receiver gain manually.
On the transmitt side I am only looking to generate a CW tone, again no modulation. The transmitter output power is flexible, preferrably in the range of 0dBm.
Almost all the parts I find on TI product portfolio have an internal modulator/demodulator for a specific scheme such as FSK - this is not what I am looking for, I just want to generate a CW tone on the transmitter and receiver it with another identical chip at the above specified frequency span. Is there a part that can comply with my requirements?
Perhaps the existing FSK chips can bypass the modulator/demodulator and purely work in CW mode?
Please advice.
Thank you,
Ali