This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: CC3220SF-LAUNCHXL: TIDC-01002 - Sub 1 Ghz Reference Design Question

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: CC3220SF

Following the white paper on this I've got everything up except for the sub 1 GHZ network. When I log into the IBM Bluemix page it shows Network Mode: Not Started. Any ideas on this?

  • Can you share the serial console prints from the CC3220SF?

  • C: Net 0, Raw Error -1, Time Out: Y [669]
    C: FH-B1 0xc0 to net 0, Sent (2 Bytes) [@ 669]
    C: Rcvd msg Fix-Hdr (Byte1) 0xd0 from net 0 [@ 669]
    C: Msg w/ ID 0x0000, processing status: Good
    C: Net 0, Raw Error -1, Time Out: Y [694]
    C: FH-B1 0xc0 to net 0, Sent (2 Bytes) [@ 694]
    C: Rcvd msg Fix-Hdr (Byte1) 0xd0 from net 0 [@ 694]
    C: Msg w/ ID 0x0000, processing status: Good
    C: Net 0, Raw Error -1, Time Out: Y [719]
    C: FH-B1 0xc0 to net 0, Sent (2 Bytes) [@ 719]
    C: Rcvd msg Fix-Hdr (Byte1) 0xd0 from net 0 [@ 719]
    C: Msg w/ ID 0x0000, processing status: Good

  • Hi Nicholas,

    Could you share the entire log from your console? preferably on a txt file so I can take a look at what could be going wrong.

    Thanks,
    Hector

  • Hector -

    I apologize for my very late reply. I was using a 1310 instead of a 1350. I was under the impression these were interchangeable. It works great with the 1350 but I'm going to working on getting it working for the 1310.