My application is for a turn-around tracking or sequential ranging system where two chips are used . One chip would only receive and the other would only transmit. However, the data from the receiving chip must be passed to the transmitting chip. Can the CC430 chips be configured as a master/slave pair or simply to pass data between them?