Hello -
I've been attempting to add an additional field to receive on the gateway. I've been trying to follow the reference code and I thought it was pretty straight forward. The problem I'm running into is that when I add an additional field to collect, I get the following error:
Version: Client LIB 1.1.0, Common LIB 1.2.0.
C: FH-B1 0x10 to net 0, Sent (72 Bytes) [@ 145]
C: Rcvd msg Fix-Hdr (Byte1) 0x20 from net 0 [@ 145]
C: Cleaning session for net 0
C: Msg w/ ID 0x0000, processing status: Good
C: FH-B1 0x82 to net 0, Sent (39 Bytes) [@ 146]
[Provisioning ERROR] - FATAL ERROR: Driver Abort detected