Other Parts Discussed in Thread: CC1310, SIMPLICITI
Tool/software: TI-RTOS
I am currently using the [node] - [concentrator] example. (board: cc1310 launcherpad)
I want to attach 200 nodes to one concentrator.
The data packet is 17 bytes and LRM will be used.
The data transfer cycle is 10 seconds.
1. Is it possible to attach 200node?
2. If 200 nodes are tough, what is the approximate number of stable nodes ?
And I saw the thread below.

3. If I use a TI 15.4 stack, can I reliably use 50 nodes with the conditions mentioned above? (17byte,LRM,10s interval)
Thanks.