Other Parts Discussed in Thread: CC2650, CC1350
Hi,
I want to establish a Start topology network which consists of 4 x Peripherals(CC1350STK) sending continiously accelerometer data (every 100ms) to the central node(CC2650 launchpad) which is connected via USB to the PC. Important is that the central should be able to connect simultaneously to the four peripherals so that they can send the accelerometer data via Bluetooth.I flashed the firmware of HosTest App on the CC2650 launchpad and I was able to connect 1xCC1350 Sensortag with the central (CC2650) via BLE-Device Monitor and to receive the data. Then I wanted to add more Peripherals, up to 4 but with the HostTest firmware on the Central, but it is not possbile to have multiple connections simultaneously with the peripherals. So I wrote to TI support and they proposed to use the firmware multirole for the CC2650 launchpad, so that the central node is able to have mulitple connections at the same time, in combination with putty or BLE-Device-Monitor or BTool. I tried it ou but I was only having a connection with putty and the problem is that Iam not able to receive the sensor data from the peripherals. Do you know how I can create such a network where 4 periherals can be connected to a central and are capable to send sensor data, so that I can display it on the screen? I gave a look but the information that I found on Ti is not complete.