Hello,
I design a motion sensor from TIDA-00489 reference design, it includes PIR motion sensor connects with CC1310 RF MCU. So when I test it the PIR sensor output remain always high, so that It can not detect motion within it's area. Then I check output from IRS-B210ST01-R1 IC (It is used in reference design for motion sensing) , the output is 637mV. Then I check waveform of PIR_OUT_HI and PIR_OUT_LOW. I did not change any circuit design and components.
I have attached schematic and waveform of it.
So please suggest some solution for that.
Thanks.