Part Number: CC1310
Tool/software: TI-RTOS
I have a question.
I am currently using two external crystals on my custom board.
I saw the following in the reference document:
-A 24-MHz external crystal is required as the frequency reference for the radio. This signal is doubled internally to create a 48-MHz clock. ( X24M_P input and X24M_N output pins.)
-The 32.768-kHz crystal is optional. The low-speed crystal oscillator is designed for use with a 32.768-kHz watch-type crystal. (X32K_Q1 input and X32K_Q2 output pins)
Each external crystal is connected to a pin. (X24M_P , X24M_N ,X32K_Q1 , X32K_Q2 )
but I know that I need to set the software in order to use an external crystal.
Can you explain in detail how and where to set it up?
and Is there a way to check if it is actually in use after setting the external crystal?
Thank you.