Other Parts Discussed in Thread: CC1352R, , CC1312R
Tool/software: TI-RTOS
Hello everybody,
at the moment I am using a CC1310 launchpad combined with a PIR sensor imitating the TIDA 00489 functionality. Using a second CC1310 launchpad and SmartRF Studio I am able to verify my code. We now want to go bigger using a star layout (many sensors + collector) and I would like to use my code again just being wrapped in some other layer for IoT. I do now have some questions what approach you would think makes most sense. I am a beginner in C/C++ and SimpleLink technology, but so far I am satisfied and I want to use it for our company. We are using the TIDA 00489 design for the sensors and the CC1310 launchpad+raspberry for collector+gateway. Basically, the sensor only sends his ID + Integer Value once in a certain time frame (periodically, but with breaks due to going into sleep mode). The sniffer receives the messages and immediately posts it on the serial interface. Now a few questions.
- How many devices are supported in one network/setup 50/100/1000?
- What happens if two devices are sending simultaneously? (Is there some kind of ACK and one sensor is sending until he receives the ACK?)
- Is there some kind of security layer hindering the correct interpretation outside of the network?
- What do you think fits better for my purpose:
- Properitary RF using basic Rx/Tx (I think this is more or less the case in the TIDA 00489 software code example)
- EasyLink
- Stack 15.4, which I think is attractive looking into the sensor/collector example though I have no clue where to put in my code...
Regarding questions 4, I would be grateful for some pros and cons of the technology and will be happy about a link to further good example/documentation. I will be diving once again into the sensor/collector example to get a better understanding.
kind regards
Stefan