This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SMARTRFTRXEBK: The board will not detect the radio chip inserted

Part Number: SMARTRFTRXEBK


Hello.

I've got two TrxEB development board with a 868 MHz radio. One of the boards will not detect a inserted radio chip. The LED above the enable/disable switch i just blinking. When i connect to the SmartRF Studio app the TrxEB board is detected but claims that no chip is present. But when i switch the radio board from one board to the other the error is the same, so the problem must be with the TrxEB board. 

Is there a way to fix/reset this error? Or do i need a new board?

Regards

Henrik