Part Number: CC1310EMK
Background:
I have previously built CC1310 solutions and I am looking at interfacing with a CC1010 based solution over the air. I do not have any experience with the CC1010 platform therefore I am looking for guidance on the compatibility between to two. A brief look at the CC1010 datasheet reveals FSK modulation, preamble, 1 byte sync, ... and the CC1310 offers flexibility to configure these settings.
Questions:
Is it possible for the CC1310 to communicate with a CC1010 over the air?
Are there any known incompatibility between these devices?
Is there any literature that might provide insight into configuring the CC1310 in a mode that is compatible with the CC1010?