Other Parts Discussed in Thread: CC1350
Hi,
I've been doing some research on the TI 15.4 for using with the CC1310 and i've a question related to the implementation of the CSMA-CA algorithm. I've previously worked with CSMA-CA in the AT86RF212B from Atmel. Using that IC, user can specify different modes to detect a clear channel as specified by IEEE 802.15.4. Below is a capture of the datasheet with the available modes.
I was wondering if there is a way of configuring the CC1310 in any of those modes. I actually need to implement mode 3 (Carrier sense and energy detection above threshold). I'll really appreciate the help.
Regards