Other Parts Discussed in Thread: CC1120, CC1190
I've just obtained the BOOSTXL-CC1120-90 EVal kit and connected it using smart RF studio. following the instructions in swra492, I have:
- Place Jumper on P6-1 to P6-2
- Place Jumper on P6-3 to P6-4
- Place Jumper on P6-7 to P6-8
- Place Jumper on P6-11 to P6-12
- IOCG0 = 0x73 in SmartRF
- IOCG2 = 0x33 in SmartRF
I'm transmitting at 915MHz which is in the middle of the band, Smart RF studio thinks the output power should be 26dBm, which matches the data sheet, however, I am only seeing a transmission of around 5-8dBm through cabling. I've tested the cable with other products and they seem to be fine, so I'm a bit curious as to why I'm not getting the correct power from the device.