This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: where is the patch for CC1310 1.5Mbps datarate

Part Number: CC1310


Hi all

   I found these words below is in the link https://e2e.ti.com/support/wireless_connectivity/proprietary_sub_1_ghz_simpliciti/f/156/p/628551/2363574 ,

       Hello Will, 

The patches needed for 1.5mbps mode on CC1310 are included in the latest SDK release and we are working on adding this mode to SDK examples.

In the meanwhile, we are working on providing settings needed to implement this mode in the next week. However, this has been characterized

at 915MHz and only tested for functionality at 433MHz under typical condition. 

I want to which version SDK  and which example include the patch for 1.5Mbps for CC1310. Is there any body know that?

Thanks a lot!