Other Parts Discussed in Thread: CC1120
We want to connect our prototype board via UART to the SMARTRF TRXEB so we can control the CC1120 EM board on the TRXEB using the MCU on our board.
Our prototype board exposes a UART port.
I know that we can control CC1120 EM board by hooking up the SPI and GPIO pins connector P7 of the TRXEB, but it is possible to connect using the UART TX and RX pins that are exposed from our board?
I basically want to bypass the MSP430 and talk to the CC1120 in a similar way to Smart RF mode, but I don't want to connect via SPI lines as I cannot cut tracks on my board and re-route SPI and GPIO lines.
regards
Sudesh