This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1312R: ZIGBEE example for CC1312R?

Part Number: CC1312R
Other Parts Discussed in Thread: CC2652R, CC1352P, Z-STACK

Tool/software: Code Composer Studio

Dear All,

At first,  I started a ZigBee project with cc2652r, but it's range is not enough, so I searched TI homepage and found that cc1312r supports ZigBee.

I already bought the cc1312r launchpad and cc1312r chipsets. And tried to start a new project for cc1312r and Zigbee, but I can't find any example project in "simplelink_cc13x2_sdk_2_30_00_45" and  "simplelink_zigbee_sdk_plugin_2_20_00_06".

Which example project should I select for cc1312r to implement the ZigBee project?

And Which 'TI explorer ' do I have to use?

Thanks.

BR,

Sean.