Part Number: CC2530-CC2591EM-RD
Hello everyone,
While rebuilding an application with IAR 8.20.1 and TIMAC 1.5.0, I'm getting the following error
Error[e16]: Segment SLEEP_CODE (size: 0x9 align: 0) is too long for segment definition. At least 0x1 more bytes needed. The problem occurred while processing the segment placement command
"-Z(CODE)SLEEP_CODE=_SLEEP_CODE_SPACE_START-_SLEEP_CODE_SPACE_END", where at the moment of placement the available memory ranges were "CODE:7ff8-7fff"
Reserved ranges relevant to this placement:
CODE:7ff8-7fff SLEEP_CODE
BIT:0-7 BREG
BIT:80-97 SFR_AN
BIT:a8-af SFR_AN
BIT:b8-c7 SFR_AN
BIT:f8-ff SFR_AN
I am using the subsequent extended command line file (with checked Override default option)
ti_51ew_cc2530b_ota.xcl
In General Options - Target I specified Device CC2530F256, Code Model Banked and Data Model Large
Part of the .xcl file
// Sleep PCON instruction must be 4-byte aligned.
//
-D_SLEEP_CODE_SPACE_START=(_CODE_END-7)
-D_SLEEP_CODE_SPACE_END=(_CODE_END)
-Z(CODE)SLEEP_CODE=_SLEEP_CODE_SPACE_START-_SLEEP_CODE_SPACE_END
Can anyone please help? Thank you!