This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1201: CC1201 how to cfg 625ksps on 2fsk

Part Number: CC1201


HELLO ,

CC1201 how to cfg 625ksps on 2fsk? 

  • I could not find any test done with this datarate. You should try to use the same method that was used with the 1.25 Msps which I sent you a link to. Start from the 500 kbps settings and increase the datarate to 625 kbps. 

    It could be that FS_DIG0 and AGC_CFG2 and the deviation have to be adjusted but you have to do tests yourself to see what you have to change to get the wanted performance. 

  • in the document cc1201.

    section 4.5: 

    data rate: 1250kbps means the 4GFSK max data rate.

    does the 625kbps means the 2fsk max data rate?

    in the rf studio7 software , the max data rate is 500k in the 2fsk mode.

    i cannot cfg the data rate exceed the 500k in the 2fsk mode?

  • SmartRF Studio is giving you a warning since 500 kbps is the highest datarate we have tested. Since 1250 kbps is tested using 4-GFSK it should be possible to use 625 kbps 2-FSK but as said you have to do testing to check the performance.