Hi,
just received the DK2, some impressive new designs!
#1 coin cell: I guess the name is just because of the size, but one has to keep the area clear from a real coin cell? One could think to stack a coin cell just above the antenna design. But where is the feed point & space for the circuit?
All others: the ground plane size will have a certain impact. If one change it, matching has to be adjusted?
#7 169MHz metal-PRO antenna: never seen something like that before. But it could be interesting fpr 434/868/2.4 too - we always have the problem to get out of the metal housings in new designs. I f we could design in the antenna into the housing, this could have advantages. Any hints for designs in these frequencies?