This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101: CC110L Evaluation card for 868-915 Mhz?

Part Number: CC1101
Other Parts Discussed in Thread: CC110L, SMARTRFTRXEBK, CC1120

Team,

Customer is looking for evaluation card for both CC1101 and CC110L.
The goal is to do some evaluation in the following band: Base freq. 867.999 Mhz, channel spacing 199.95kHz , carrier 867.9Mhz, GFSK mod, 0 dBM TX power.

It seems that the CC11XLDK-868-915 kit is not available anymore.
What kits the availlable (ie orderable and in stock)?

Looking at CC1101:
http://www.ti.com/product/CC1101/toolssoftware#desKits
The SMARTRFTRXEBK is in stcok but the CC1101EMK868-915 daughter card is not.
-Is it possible to get some CC1101EMK868-915 daughter cards?
-Is there a BOOSTERPACK available for CC1101?

Looking at CC110L:
http://www.ti.com/product/CC110L/toolssoftware#desKits
The SMARTRFTRXEBK is listed but it does not seem that a compatible module is available.
-Is there a compatible CC110L daughter card available?

The 430BOOST-CC110L is listed as well.
-Can it support the above sub-1Ghz parameters?
-What MCU lauchnpad do we recommend?
-With which MCU launchpad are the SW examples (PER test SW, CC11xx example libraies, ..etc) compatible?
-Do we have ready to use examples for MCU launchpad + 430BOOST-CC110L? any example for MSP430FRxxx launchpad?

CC13xx is not an option as an other MCU is used already. Just the sub-1Ghz transceiver is needed.

Thanks in advance!

A.