Part Number: 430BOOST-CC110L
Tool/software: WEBENCH® Design Tools
Hello,
I'm using CC110L BoosterPack with stm32, I want to send the data from the Master (STM32 &CC110L) to slave receive (STM32 &CC110L) with IDE EWARM.
I configured the master with frequency 868 MHz to send the data to the slave.
The command SPI passed with successfully to RF Module CC110L and the RF module send the data as he shows the figure 1 on SDR.
my problems are (always the frequency is 868Mhz)
1 - the master sends data, but in slave I can't receive this data withe two (STM32 &CC110L)
2 - the same code works for send and receive data in Code Composer Studio with two launchpad (MSP430 & CC110L)
3 - Not data Recieve when I configure the slave with the (MSP430 & CC110L) te receive the data sent from the master (STM32 & CC110L)
4 - In MSP430 the frequency 902Mhz works but in STM32 not work
figure 1 : data sent from master STM32 & CC110L
figure 1 : data sent from master MSP430 & CC110L