Part Number: 430BOOST-CC110L
Hello,
I've bought the Launchpad MSP-EXP430G2ET together with the
AIR Boosterpack and tried to connect it to "SmartRf Studio". I've
rotated the UART headers. The drivers are: "MSP Application
UART1 (COM4) - C:\WINDOWS\system32\DRIVERS\usbser.sys"
and "MSP Debug Interface (COM3) -C:\WINDOWS\system32\DRIVERS\usbser.sys".
When I push the button on SmartRF Studio
"Find device" the red led on MSP430 flashes short, bat it shows no
device. What is wrong?
Thanks for any help.
Best regards
Thomas