HI everybody
I am working with the cc1010. My problem is that I have evaluation board and two evaluation modules. In swru055 I have read that PC running Keil compiler and
Chipcon IDE and we can use parallel port to download debug monitor to cc1010 evaluation module through evaluation board. When I use Keil uVision3 I see that we can not download program to cc1010 using Flash menu. I try to find CHipcon IDE (may be flash progammer) for cc1010 but I can not find in TI webpage. Anyone can tell me where is the IDE software of cc1010 to download.
Also I want to make a test program to blink LED on IO pin of cc1010 through evaluation board. Anyone tell me if it is okie to do this