Hello
I am trying to configure a CC110L transceiver. I configure all the registers and after I read them in order to check the values are correct, and they are.
Then I send the command strobe STX with FS_AUTOCAL=0X01 configured.
The value of MARCSTATE goes to 0x13 which is ok for STX state but the FSCAL1 value is 0x00. It has changed from 0x3F to 0x00 but I suspect this is not a good value, and the transceiver does not send anything.
Any idea which could be the problem? I check also the MARCSTATE value since I send the STX command and see that the values are 0x08 (CALIBRATE) , 0X09 (BW_BOOST) and 0x13 (TX ON). I don' see 0X0A sate whcih is supposed to be FS_LOCK, but not sure if I should see it.
Thanks for your help in advance