Hello Sir,
I am using the CC1350 SensorTag (Peripheral) and a CC1350launchpad connected via USB on the Computer. I flashed the Host APP on the Launchpad and used the BLE-Device Monitor to read out the sensor of the CC1350 STK via Bluetooth Low Energy and it worked fine. After that, I have tested it via the smartphone using the TI Sensortag APP and it worked fine.
My target is to modify the firmware of the CC1350STK sending only some SensorData and to set up the intervals of reading out the sensors. My question was where I could find the same factory firmware that is flashed from the sensortag when it is delivered. I saw that several people using the CC1350STK are facing this problem and they are several threads here.
So Tell me sir where will i get zip file for firmware update of the CC1350STK