Part Number: CC1310
Other Parts Discussed in Thread: ENERGIA, TIDC-01002, ENERGYTRACE
Dear All,
After implementing the solution for sub1 GHz collector (MSP432 + CC1310 launchpad as co-processor) and another CC1310 as sensor, and using the example projects, provided by TI (described in details in answer of my previous and related to this one post, I was able to connect the sensor and the collector but no information for the ambient temperature, etc. is received.
This is the sensor monitor -
Starting...
State Changed: 1
Started: 0x1
Channel: 1
State Changed: 3
and this is the collector one:
----------------------------
SimpleLink 15.4 Stack Collector Demo
----------------------------
Collector init complete
Started
Channel: 1
PermitJoin-ON
Joined: 0x1
Can you help me to figure out what is the issue?
Thank you and best regards,
Stanislav