Hi, I'm working with the TX-RX examples located inside the CC1310 SDK. I have implemented communication via UART and it works very well. Now I am implementing a new topic: I have two boards that speak and work, if I do not feed one board and with the other I send the command .... can I turn on an LED if it is not received?
Thanks!