Tool/software: Code Composer Studio
Hey guys,
since AB seems to be out of office and certification starts next week I repost the question regarding the input for a questionnaire, which is needed by the certification lab.
The whole questionnaire can be found in EN300 200-2 v3.1.1 2017-02 in Annex D.2 (pp. 28). On page 29 the following questions appear:
h) What is the spectrum access mechanism of the equipment? -> Polite spectrum access (My answer)
i) In case of polite spectrum access:
- The CCA time implemented by the equipment is ........ ms.
- The minimal unit of deferral period is: ..........
- The deadtime T_DIS is ............ ms.
Could you provide me with the answers?
My config settings:
/*! MAC Parameter */ /*! Min BE - Minimum Backoff Exponent */ #define CONFIG_MIN_BE 3 /*! Max BE - Maximum Backoff Exponent */ #define CONFIG_MAX_BE 5 /*! MAC MAX CSMA Backoffs */ #define CONFIG_MAC_MAX_CSMA_BACKOFFS 4 /*! macMaxFrameRetries - Maximum Frame Retries */ #define CONFIG_MAX_RETRIES 1
If you need any further info please let me know immediately.
Best wishes
Slev1n