This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1310: CC1310 consumption

Part Number: CC1310


Tool/software: Code Composer Studio

Hi there, I have a problem with a CC1310F128RHB based board. The problem is that when the radio chip is in RX mode (using EasyLink_receiveAsync function) it consumes 20 mA (6 mA by CPU and 14 mA by rx radio). Datasheet says that radio in RX mode consumes 5.4 mA. Where can be the problem? Thanks.