This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352R: Mioty Sensitivity

Part Number: CC1352R
Other Parts Discussed in Thread: MIOTY,

Hey community,

I would like to know about the expected sensitivity for the use of mioty with the cc1352R. 

In the datasheet, I can find the sensitivity values for the use of the IEEE 802.15.4g (-110 dBm) and the SimpleLink LRM (-121 dBm).

But I can't find information about the mioty sensitivity. 

Is there a document I can refer to? 

thanks in advance,

Thomas

  • Hi,

    Preliminary answer is the sensitivity limit will be equal or better than -121 dBm.

    Will confirm the exact level soon.

    Regards,

       Richard

  • Hi Thomas, 

    Unfortunately, the mioty parameters are not in the datasheet but I can share some preliminary results with you. The preliminary results for CC1352 are in the range of about -128 dBm @ 10% PER (Core, No Repetition, -127 dBm at 255 Byte Downlink). This can be improved by about 0.5 dB by increasing the LNA current somewhat.

    Thanks, 
    Elin