Other Parts Discussed in Thread: WMBUS,
Hi,
I struggle with the max number of supported meters as a collector in the wMBus Stack of Stackforce in combination with the CC1310.
Where is the reason for the limitation of 16 meters? Is it because of the hardware or is the limitation in the stack?
And is it possible to use more meters with another Hardware or another version from StackForce?
I think a possible solution could be the deactivation of the "address filtering" property in the collector. Then all received telegramms are forwarded to the application layer. Then the mapping to known meters and the encryption would be done by our own code but it could be possible to work with more meters than 16.
Do you know anything about limitations with that deactivated address filtering?
Or where could I ask for more information?
Related Forum Threads:
https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz/f/156/p/687323/2537578#2537578?jktype=e2e
and
Thanks
Best regards
SB