Part Number: TI-15.4-STACK-GATEWAY-LINUX-SDK
We have two CoP module builds, one uses cc1310 simplelink cc13x0 sdk 4_10_00_10 for E70 cc1310 module as CoP, another uses simplelink cc13x2 26x2 sdk 4_30_00_54 for E70 cc1312 module as CoP.
The host chooses Linux x64 sdk 4_20_00_05. We ported to mips platform and run well.
Two questions:
1. I found tx power for host + cc1310 CoP has normal value (10.x dBm), but host + cc1312 CoP has abnormal value (2.x dBm). No matter the config-tx-power is set to default 14 or 13. Is it the compatible issue?
2. I see TI 15.4 stack version is different for Linux x64 sdk 4_20_00_05 (3_20_00_00) and sdk 4_30_00_06 (3_30_00_00). Not sure why it matters with TI 15.4 stack version. Supposed to be CoP?
Peter.