Hi there,
I have a question about the frequency offset compensation behavior after the auto calibration done.
According to the CC113L datasheet, when FOCCFG.FOC_BC_CS_GATE=1 is set and the receiver is in no signal condition (the CS signal is low), the frequency offset compensator will freeze and the offset information obtained is maintained.
In this situation, if state change operation below inclusive the calibration is done, is the offset information in (1) taken over to (4) or reset to the center frequency?
(1)RX state with CS signal low --> (2)IDLE state --> (3)Calibration --> (4)RX state with CS signal low
If it is reset to the center frequency, is there any way to take over the offset information to (4)?
Best regards,
Sinsan