Hello,
I am using a custom board with CC1310 RSM package, and I am trying to put it in Standby mode, but the current consumption is around 2.5 mA.
I have tried the pinStandby example in the launchpad and it is working. But on the custom board with CC1310 RSM it is not working (I disconnect the jtag..).
I have verified that there is no leakage current because when I adapted the pinShutdown example on the custom board the current was in the micro amps (as expected).
My pin setup is as follows:
IOID_0 2 3 4 not connected
IOID_1 to LED through resistor
IOID_5 7 Digital input (pulled high by an external resistor)
IOID_6 analog input
IOID_8,9 I2C (pulled up externally by 4.7 kohm)
I have verified that all pins are working (tested DIO, tested I2C) so the board.h and relevant .h .c files are changed in a correct way (as far as I can tell).
My question is does the Standby mode work for RSM package. Is there anything special that needs to be done to adapt the examples for the launchpad to the RSM package.
Am I missing something?