Hi,
I need to size crystal accuracy for 433.92MHz receiver application with a CC1200.
For this, I'd like to take into account the frequency drift of emitter and thus its crystal accuracy.
I tried to do this with the following formula that I found in the application note SWRA122:
BW channel > BWsignal + (4 × XTALppm × fRF)
However, this formula seems to be available in case of same ppm of the crystals for the emitter and the receiver, which is not my case.
Here are my features:
Emitter:
- Xtal ppm: 55ppm
- Carrier frequency: 433.92MHz
- Frequency shift: +-25kHz (deviation 50kHz)
Receiver:
- Carrier frequency: 433.92MHz
- RX filter: 300kHz
How deduce Rx crystal ppm with this features?
Best regards
Martial